|
Promotional Part Number:HD64F36077GFZV
The H8/36077 Group offers enhanced fail safe functions (oscillation stop detection function: the watchdog timer starts operating after the reset state is canceled) based on the H8/3687 Group. Peripheral functions match those of the H8/3687 Group, including a 16-bit timer with two channels, a two-channel asynchronous/synchronous serial interface, and a one-channel I²C bus interface. This group can be used for to motor control thanks to the added 2-channel 16-bit timer. Moreover, it can also be used for network-connected home appliances by employing the two-channel serial communication interface and one-channel I²C bus interface.
|