HI2000/3 Real-time OS for H8S Family (Discontinued product)
Target device
The H8S family
Overview
University of Tokyo Professor, Ken Sakamura advocated TRON project in 1984. The µITRON specification is a one of the specification of the real-time operating systems which was standardized in the ITRON project established as a subproject of the TRON project.
The µITRON specification is now a de facto standard in the Japanese embedded industry.
Renesas Electronics Corp., has been participated in the TRON project up to this day since the project was established. [HI series OS] is a realtime operating system for the Renesas H8/SH microcomputers which is compliant with µITRON specifications.
Refer to the TRON Association website for detailed information on the ITRON spescification and the µITRON specification.
ITRON Project Home Page
*T-Engine Forum holds the copyright on the μITRON Specification.
*TRON, ITRON, and μITRON do not refer to any specific product or products.
Singapore/South & Southeast Asia/Oceania