Skip to main content

image

Microcontrollers and kit solutions supporting AUTOSAR software drivers, for optimal body control

Body systems are making ever more extensive use of electronics to provide enhanced vehicle comfort and safety. Examples include power windows, automatic air conditioning, systems for controlling the seat position to match the driver, headlight illumination control linked to the steering angle, and anti-theft systems. In order to meet these diverse and varied requirements, there needs to be support for integration and reuse across systems. For example, the lineup of MCAL* for Renesas automotive MCUs satisfying the latest AUTOSAR standard is being expanded. Use of the AUTOSAR standard enables development work spanning different vehicle body types and models. This allows increased system stability, better quality, and reduced cost through economies of scale. In addition, the popularization in recent years of HEVs and EVs is increasing demand for lighter weight and reduced dark-current noise in body systems due to their direct connection with battery performance.
Renesas responds to these requirements with kit solutions for optimal body control combining MCUs, analog devices, power devices, and so on.

* MCAL: Microcontroller Abstraction Layer

Roadmap

Body Roadmap

R8C/5x 78K0/Fx2-L 78K0S/Kx1+ R8C/3x R8C/2x RL78/F12 78K0R/Fx3 78K0/Kx2 78K0/Fx2 V850E2/Fx4-L V850ES/Fx3-L V850ES/Fx3 V850E2/Fx4 RH850/F1L RL78/F1x RH850/F1x V850E2/Fx4-H

Lineup:

Renesas Automotive Product Catalog


End of content

Back To Top